Following_error_time_out
Index.Sub | 6066.0H |
Data Type | Unsigned16 |
Access | Read/Write |
PDO Mappable | No |
Unit |
milliseconds (ms) |
Range |
Unsigned16 |
Default Value | 0 |
Store Supported | No |
Description | When the following error occurs longer than the defined value of the time-out, the corresponding Bit13 (following error) in the Statusword will be set to one. |
Notes |
-- |